This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSCNCD28335: CCS/TMDSCNCD28335

Part Number: TMDSCNCD28335


Tool/software: Code Composer Studio

Hi, 

I am using TI F28335 DSP to run a three phase induction motor. The project I am using is HVACI_Sensorless_2833x. I want to change the dead band value in the program but it seems I can not find the specific code in this project to change it. I am using Build level 1 to run the motor. I would appreciate if anyone can help me in which file I need to bring the change. 

Regards

Ashik