Part Number: IWR1642BOOST
Other Parts Discussed in Thread: UNIFLASH, , IWR1642, AWR1642
Tool/software: Code Composer Studio
Hello, uniflash team,
I have a test in TI IWR1642BOOST, I want to download the demo package BIN file(xwr16xx_mmw_demo.bin) via UART directory in UniFlash(5.0.0) without usb(connect with XDS110),
(1) Modify the IWR1642BOOST Hardware, remove the R128 and 129, connect the R169 and R166 with 0 Omh resistance,as below,
(2) Select the Flashing Mode(101),
(3) Used a FTDI to USB adapter to connect PC and iwr1642 UART(RX: Ball N4 / TX: Ball N5 ) through J6(Pin 5 and Pin 7).
(4) Used a 5V/2A power adapter to supply Power, then connect [FTDI to USB adapter] to PC. Open uniflash tool to download BIN file.
But it could not download, the error code as above!!!!
I have posted the issue in Sensors forum(e2e.ti.com/.../3028358
the TI Engineer in the Sensors forum let me check with the uniflash team by posting on the Tools forum to comfirm if the USB adapter is compatible.
Could you take some suggestions?
I am waiting for your reply, it is very very Important for me.
Regards,
Eric