Part Number: LAUNCHXL-CC1350-4
Other Parts Discussed in Thread: CC1350
Tool/software: Code Composer Studio
Hi there,
I am trying to build and debug a project to my CC1350 Launchpad using Code Composer Studio version: 9.1.0. The example I am trying to build is "rfSynchronizedPacketTx_CC1350_LaunchXL_tirtos.ccs. This can be found in my TI project directory for code composer studio. If you would like to know the exact path, then just check the screenshots below.
I have already checked my target configurations and the Launchpad is connected successfully.
The error: The error itself is something to do with gmake which can be seen in the build console (second screenshot).
The first screenshot is just the standard console. Not much information here but it might help at some stage.
The second screenshot is of the build console.
The third screenshot is the project overview, where I have 2 projects; one is labelled as RTSC and the other is CSS. The CSS project has a noticeable red cross in the corner of the icon. It is worth noting that the CSS project "rfSychronizedPacketTx_CC1350_LAUNCHXL_tirtos_ccs" is the one that isn't building, however the RTSC project "hello_CC1350_LAUNCHXL_tirtos_ccs" builds/debugs just fine. Originally I thought that the problem was with the RTOS projects since all of the NORTOS projects I have tried, build first time. So that is not the case.
The fourth and final screenshot is of the actual error popup I receive straight after I start a debug process.
Thank you. I Hope to hear back from somebody soon with a possible solution. Please note I am new to this software and the launchpads. And embedded systems programming as a whole. Will try my best to get this sorted on my own accord also.