Other Parts Discussed in Thread: SEGGER
Tool/software: Code Composer Studio
Hi, Ti E2E Team,
In the "ARM® Cortex®-M4F-Based MCU TM4C1294 Connected LaunchPad™ Evaluation Kit", I disconnect the 0 Ohm resistance in JTAG line between TM4C1294NCPD and TM4C123G.
Connect the TCK, TMS, TDI, TDO, RESET, GND, 3.3V in TM4C1294NCPD to TCK(pin9), TMS(pin7), TDI(pin5), TDO(pin13), RESET(pin15), GND(pin4), VTref(pin1) in J-Link.
Open the CCS project in CCS v8 software, then click "Run->Debug", the following picture appears,
Then I select the "SEGGER L-Link Emulator/CORTEX_M4_0(Disconnected: Unknown)", right click and select the "Connect Target", it shows,
It seens connect, but can not debug in main.c file(such as take a break). I have searched in SEGGER about J-Link connecting with CCS(https://www.segger.com/products/debug-probes/j-link/technology/ides/ti-code-composer/), I modify the configuration as below,
I want to know why it can not connecte? Are there any other collocations in CCS?
I am waiting for your reply.
Thank you.
Regards,
Eric