This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: Error encountered during linking

Part Number: TMS320F28335

Tool/software: Code Composer Studio

I am working on PI controller for a DC-DC converter. The following errors showing-

  • Hi,

    The error messages clearly show that you have lots of symbols defined at least two times in the files that comprise your project (redefined symbols) - it even says which files have them. The _pi1 symbol is found in Adc.c and also redefined in DefaultIsrnonBIOS, ECap, EPwm, and so on.

    Usually this is due to conflicting libraries and source code, but given there are too many errors of the same symbol, this indicates that an #include file is not declaring but may be instead defining this symbol. The third reply on this thread talks about this.

    --Cheers