Tool/software: Code Composer Studio
Dear Support:
We are using the TMSF28069M device and have 3 of them daisy-chained together and trying to download code to them using CCSv8.3 and CCSv9.1 and getting some rather bizarre behavior that I was hoping you could explain. When pressing the debug button to download code, we have no issues downloading to the 1st and 2nd device, but when we get to the 3rd device it always fails. So we go to the method of launching the .ccxml file and we connect to each CPU individually and again - no issues connecting to the 1st and 2nd devices, but when we get to the 3rd device it fails. So we retry again and it fails. However when we retry a 3rd time, it connects. I have done this hundreds of times and it is consistent. Once we connect to this 3rd device, we have no issues downloading the code and running.
This doesn't sound like a noise or signal integrity problem since it is so reproducible and once we connect, we have no issues with downloading the code. Is there anything that we might be missing in setting up the debug configuration such that we have to do something special to the last device in the chain so we can download reliably and consistently to all 3 devices the 1st time and not have to go through retries to this last device in the chain? Your thoughts?
Thanks,
Tim