This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AM3359: NDK project example

Part Number: AM3359

Tool/software: Code Composer Studio

There does not seem to be a clear project path to use the NDK that I can see. I have built the libs and see everything in NDK core stack (cfg) file. As I go thru the documentation  I add more files for hardware and stack links, but that end up need more and more files added to the project as I add these file more get requested. I don't see anywhere a simple project that would just allow me to build (CCS with RTOS) and ping the board. Is there one?

compiler 18.12.2.LTS

BIOS 6.73.12

NDK 3.40.1.01

XDC 3.50.7.20.core

Any help would be great!