This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443BOOST: about mmWave SDK

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

Tool/software: Code Composer Studio

Hi There

I have a IWR1443BOOST, the device version is ES2.0

and I installed mmWave SDK 3.2.0.4

I have some questions.

1. I want to test the mmWave SDK Demo program ( 14xx - mmWave SDK Demo ) 

    But it supports mmWave SDK 2.1.0.4 and IWR1443 ES3.0.

    Can't I test the demo program because my IWR1443BOOST device version is ES2.0 ?

   

    Can I compile the demo program using mmWave SDK 3.2.0.4?

    If the demo program must be modified to be compiled, what should I modify?

    could you explain it in detail?

 

2. Most of demo programs for mmWave Sensors is for low sdk version (  below 2.1 )

    How can I compile the demo programs with mmWave SDK 3.2.0.4?  

3. Is IWR1443 ES2.0 device no longer producing?

    Does it currently produce only IWR1443 ES3.0?

4. How should I get mmWave SDK 2.0 and 1.2?

I will wait for your answer.

thank you

  • Hi Son Dong-Seong,

    The ES2.0 is no longer being produced, as a result you must use the mmWave Demo out of the mmWave_SDK1.2 or earlier. ES2.0 is not compatible with SDK2.1. (For future reference IWR1443 is not compatible with SDK3.0+)

    Cheers,

    Akash