Tool/software: Code Composer Studio
Hi. Based on the UIA usage in the lab manual.
I wonder how many milliseconds this cycle represents.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi. Based on the UIA usage in the lab manual.
I wonder how many milliseconds this cycle represents.
JunYoung,
I am not familiar with the lab manual you are referring to.
Here is some general information you will need to figure out the time:
A cycle generally refers to a clock cycle (a single tick of the internal clock.) Cycles per second are also called Hertz, or Hz, thus a 2 GHz CPU (two gigahertz) goes through 2,000,000,000 cycles every second.
Thus if you know the frequency that your CPU core is running at you can calculate the time.
Regards,
John