This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCSV9 change backgroundcolour and textcolour

Tool/software: Code Composer Studio

Hello,

I want to change the background color to black and the text color to white.

What I have to do?

Best Regards Friedrich

 CCS Version: 9.0.1.00004 just updated

  • Friedrich,

    The best way to do this is probably to use what are called "Themes"

    If you go to the preferences dialog in CCS.  On Windows/Linux this is on the Window menu.

    If you expand General and select Appearance you will be able to change the theme

    Here you can try the Dark theme:

    I would give that one a try.  There is also a plug-in to Eclipse called Color Theme that some people like.  It provides a bunch more theme options.   It is available from the Eclipse Marketplace which is on the Help menu.

    Regards,

    John