This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: 0x3FE493 (no symbols are defined) when load Example_28379D_LaunchPad_demo

Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE

Tool/software: Code Composer Studio

Hi;

This error occured When I load example_demo project of tms320f28379D launchpad?

Can anyone give me your advice ?  

   

  • Which version of CCS are you using? It also appears that you are using ControlSuite and the older Resource Explorer interface to import, build and debug the project. I would recommend moving to the latest tools if possible.

    First install CCSv9 (http://software-dl.ti.com/ccs/esd/documents/ccs_downloads.html). Then you can use Resource Explorer from within CCS (it a newer interface than the one you are using) to download and install latest C2000Ware. Then navigate into the Resource Explorer to find the LaunchPad project and import it using the "Import to IDE" icon. Then build and loading to target should work.