Tool/software: Code Composer Studio
Hello,
The error below appeared during building the code with CodeComposerStudio. Could you tell me the reason ? I would like resolve this issue. I checked the NassFcm.c line 22850 as compiler told. But I belive there is no wrong code. There just a code for variable declaration.
"C:\ti\ccsv7\tools\compiler\ti-cgt-arm_16.9.1.LTS\bin/armcl" -mv7R4 --code_state=32 --float_support=VFPv3D16 -me -g --diag_warning=225 --diag_suppress=824 --diag_wrap=off --display_error_number --enum_type=int --abi=eabi --"include_path=C:\ti\ccsv7\tools\compiler\ti-cgt-arm_16.9.1.LTS\lib\src" --define=PRODUCT_NAME=NassFCM --define=PROJECT_ID="('.')" --define=MAJOR_VER=0 --define=MINOR_VER=0 --define=PATCH_VER=0 --define=FIRMWARE_PROJECT_ID="('.')" -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DMODEL=NassFCM -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO --include_path=C:/Users/ANURAD~1.WIJ/DOCUME~1/Nass/FCCTR-~1/FCCTR-~1/V4SIMI~1/Main --include_path=C:/Users/ANURAD~1.WIJ/DOCUME~1/Nass/FCCTR-~1/FCCTR-~1/V4SIMI~1/Main/NassFCM_ert_rtw --include_path=C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.1.LTS/include --include_path=C:/Users/ANURAD~1.WIJ/DOCUME~1/Nass/FCCTR-~1/FCCTR-~1/V4SIMI~1/Main/AppInterface/Nass --include_path=C:/Users/ANURAD~1.WIJ/DOCUME~1/Nass/FCCTR-~1/FCCTR-~1/V4SIMI~1/Main/AppInterface/Generic --include_path=C:/PROGRA~1/MATLAB/R2017a/extern/include --include_path=C:/PROGRA~1/MATLAB/R2017a/simulink/include --include_path=C:/PROGRA~1/MATLAB/R2017a/rtw/c/src --include_path=C:/PROGRA~1/MATLAB/R2017a/rtw/c/src/ext_mode/common --include_path=C:/PROGRA~1/MATLAB/R2017a/rtw/c/ert "NassFCM.c"
>> NassFCM.c, line 22850: INTERNAL ERROR: CONSTANT TABLE ERROR - CODEGEN ABORTED
This may be a serious problem. Please contact customer support with a
description of this problem and a sample of the source files that caused this
INTERNAL ERROR message to appear.
Cannot continue compilation - ABORTING!
>> Compilation failure
gmake: *** [NassFCM.obj] Error 1