I am running CCS v4,current. . against the Experimenters Kit with the Delfino (28335) MCU.
I keep getting interrupted by an XDS100 error %80002020/ -150. . . Where can I get more information about that error?
Will
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am running CCS v4,current. . against the Experimenters Kit with the Delfino (28335) MCU.
I keep getting interrupted by an XDS100 error %80002020/ -150. . . Where can I get more information about that error?
Will
Thanks Ki, You are fast.
I had already read that post. .and it does not seem to fit my symptoms, which is why I asked for more info on the error code itself.
That post does not include the first half of the error: e.g. x80002020/ Perhaps I should have told the whole story.
In my case; CCS connects to the card. . .downloads my dot out image and lets me set the watch points and click on the play button.
As soon as the motor makes a noise, the error shows up. Once the error happens, I have to exit CCS in order to reset the XDS100.
I have verified that all of my pieces and parts are on a common ground plane.
Will
Are you running an example that comes with the kit or is this your own app?
I am running the HVPM_sensorless_2833x, but on the Experimenters Kit hardware. The code should be almost untouched.
Thanks William. I will see if I can reproduce this.
One more thing - are you using the latest version of CCSv4? (4.2)?
You can use the Update Manager in CCS. Under 'Help->Software Updates->Find and Install'.
More data on the trouble:
When I unhook the motor, it runs ok without the error.
With the motor hooked in, I get that error.
I added the "Flashing LED" line into the code. .and it continues to blink after CCS reports the error.
I changed the incremental to Build2. . and the motor continues to turn after CCS reports the error.
To clear the error, both the Delfino and CCS have to be reset.
I need to work on tuning the PID in order to proceed. So the XDS100 needs be working.
Is there any chance that I can get the XDS100 v2?
Will Friesen