This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320C6713B: TMS320C6713

Part Number: TMS320C6713B

Tool/software: TI C/C++ Compiler

While Debugging the program using compiler version ti-cgt-c6000_7.4.24 for TMS320C6713 I got the following error message...

[Start: Spectrum Digital XDSPRO USB Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]

-----[Print the board config pathname(s)]------------------------------------
C:\Users\GURU\AppData\Local\TEXASI~1\CCS\
    ccs910\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_conf
Download failed for file C:\ti\ccs910\ccs\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
[End: Spectrum Digital XDSPRO USB Emulator_0]
Please provide solutions for this problem.
Thank You.