Part Number: MSP430F5132
Other Parts Discussed in Thread: SM72295, , MSP-FET, TIDA-00120, MSP430F4132
Tool/software: Code Composer Studio
I use CCS V. 9.1.0.0010
I made an experiment board copying the above eval. board with MSP430F5132 and SM72295....when I try to load the code to MCU i get a message "error connecting to the target : unknown device.."...I use an MSP-FET ver. 2.0.6 .....connections MSP-FET to target : ...pin 2 to vdd....pin 8 to TEST.....pin 9 to GND....pin 11 to RST.......a cap 1nF, RST to GND.....a resistor 47k VDD to RST....I suppose Spy-Bi-wire (SPW) ...why the target MSP430F5132 not recognized ? how to programming that MCU....MSP debug interface (COM9), is ok...