This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320C6748: C6748 Custom Memory Map

Part Number: TMS320C6748


Tool/software: TI C/C++ Compiler

Hi,

I have a TMS320C6748 custom board with a 256 DDR.

I made a custom memory map and currently having a problem with booting. But, it works well in simulation mode. Only troubles with flash boot. flash boot doesn't work.

I have applied some extreme values for testing purpose. mem size will be reduced in the real session. This is due to compiling USB driver.

[at the end of .cfg file]


Program.sectMap[".bss:extMemCache:ramdisk"]                 = new Program.SectionSpec();
Program.sectMap[".bss:extMemCache:ramdisk"].loadSegment     = "APP_CACHED_BIOS_RSVD_MEM";
Program.sectMap[".bss:extMemCache:ramdisk"].type            = "NOLOAD"


[local .cmd file]

-heap 0x80000
-stack 0x80000

MEMORY
{
      FLASH_CS2     org=0x60000000 len=0x02000000 /* AEMIF CS2 region */
      FLASH_BOOT    org=0x62000000 len=0x02000000 /* AEMIF CS3 region */
      FLASH_CS4     org=0x64000000 len=0x02000000 /* AEMIF CS4 region */
}

SECTIONS
{

    .aemif_mem :
    {   
    } > FLASH_BOOT, RUN_START(NANDStart)

    "CFG" > DDR_CFG

    "DDR" > DDR

    .ddrram  :
    {   
        . += 0x04000000;
    } > APP_CODE_MEM, type=DSECT, RUN_START(EXTERNAL_RAM_START), RUN_END(EXTERNAL_RAM_END)
}

[ custom Platform.xdt]

metaonly module Platform inherits xdc.platform.IPlatform {

/*config int DDR_SIZE = 0x07FF33EC;*/

config int KB = 1024;
config int MB = KB*KB;

config int SBL_SIZE = 4*KB;

config int DDR_ADDR = 0xC0000000;
config int DDR_SIZE = 10*MB;

config int APP_CODE_MEM_ADDR = DDR_ADDR+DDR_SIZE+SBL_SIZE;
config int APP_CODE_MEM_SIZE = 30*MB;

config int APP_CACHED_DATA_MEM_ADDR = APP_CODE_MEM_ADDR+APP_CODE_MEM_SIZE;
config int APP_CACHED_DATA_MEM_SIZE = 30*MB;

config int APP_UNCACHED_DATA_BLK3_MEM_ADDR = APP_CACHED_DATA_MEM_ADDR+APP_CACHED_DATA_MEM_SIZE;
config int APP_UNCACHED_DATA_BLK3_MEM_SIZE = 30*MB;

config int APP_CACHED_DATA_BLK1_MEM_ADDR = APP_UNCACHED_DATA_BLK3_MEM_ADDR+APP_UNCACHED_DATA_BLK3_MEM_SIZE;
config int APP_CACHED_DATA_BLK1_MEM_SIZE = 30*MB;

config int APP_CACHED_DATA_BLK2_MEM_ADDR = APP_CACHED_DATA_BLK1_MEM_ADDR+APP_CACHED_DATA_BLK1_MEM_SIZE;
config int APP_CACHED_DATA_BLK2_MEM_SIZE = 30*MB;

config int APP_CACHED_BIOS_RSVD_MEM_ADDR = APP_CACHED_DATA_BLK2_MEM_ADDR+APP_CACHED_DATA_BLK2_MEM_SIZE;
config int APP_CACHED_BIOS_RSVD_MEM_SIZE = 30*MB;

config int DDR_CFG_ADDR = APP_CACHED_BIOS_RSVD_MEM_ADDR+APP_CACHED_BIOS_RSVD_MEM_SIZE;
config int DDR_CFG_SIZE = 10*MB;

    config ti.platforms.generic.Platform.Instance CPU =
        ti.platforms.generic.Platform.create("CPU", {
            clockRate:      300.0,    
            catalogName:    "ti.catalog.c6000",
            deviceName:     "TMS320C6748",
            customMemoryMap:
           [    
                ["IRAM",                        {name: "IRAM",                      base: 0x11800000,   len: 0x00040000,   space: "code/data",     access: "RWX",}],
                ["IROM",                        {name: "IROM",                      base: 0x11700000,   len: 0x00100000,   space: "code/data",     access: "RX", }],
                ["L3_CBA_RAM",                  {name: "L3_CBA_RAM",                base: 0x80000000,   len: 0x00020000,   space: "code/data",     access: "RWX",}],
                ["DDR",                         {name: "DDR",                       base: DDR_ADDR,     len: DDR_SIZE,   space: "code/data",     access: "RWX",}],
                ["APP_CODE_MEM",                {name: "APP_CODE_MEM",              base: APP_CODE_MEM_ADDR,   len: APP_CODE_MEM_SIZE,   space: "code/data"}],
                ["APP_CACHED_DATA_MEM",         {name: "APP_CACHED_DATA_MEM",       base: APP_CACHED_DATA_MEM_ADDR,   len: APP_CACHED_DATA_MEM_SIZE,   space: "code/data",}],
                ["APP_UNCACHED_DATA_BLK3_MEM",  {name: "APP_UNCACHED_DATA_BLK3_MEM",base: APP_UNCACHED_DATA_BLK3_MEM_ADDR,   len: APP_UNCACHED_DATA_BLK3_MEM_SIZE,   space: "code/data",}],
                ["APP_CACHED_DATA_BLK1_MEM",    {name: "APP_CACHED_DATA_BLK1_MEM",  base: APP_CACHED_DATA_BLK1_MEM_ADDR,    len: APP_CACHED_DATA_BLK1_MEM_SIZE,   space: "code/data",}],
                ["APP_CACHED_DATA_BLK2_MEM",    {name: "APP_CACHED_DATA_BLK2_MEM",  base: APP_CACHED_DATA_BLK2_MEM_ADDR,   len: APP_CACHED_DATA_BLK2_MEM_SIZE,   space: "code/data",}],
                ["APP_CACHED_BIOS_RSVD_MEM",    {name: "APP_CACHED_BIOS_RSVD_MEM",  base: APP_CACHED_BIOS_RSVD_MEM_ADDR,    len: APP_CACHED_BIOS_RSVD_MEM_SIZE,   space: "code/data",}],
                ["DDR_CFG",                     {name: "DDR_CFG",                   base: DDR_CFG_ADDR,   len: DDR_CFG_SIZE,   space: "code/data",     access: "RWX",}],
           ],

          l2Mode: "0k",
          l1PMode: "32k",
          l1DMode: "32k",
    });
    
instance :
    
    override config string codeMemory  = "APP_CODE_MEM";   
    override config string dataMemory  = "APP_CODE_MEM";    
    override config string stackMemory = "IRAM";

    config String l2Mode = "0k";
    config String l1PMode = "32k";
    config String l1DMode = "32k";
}

What am I doing wrong here?

  • Hi Daniel,

    Can you give us more details on what is working and what is not? It sounds like when you load the application (with the above .cfg file) with CCS, it works properly. Is that correct? Please realize that the CCS .gel file may execute some things (e.g. disable watchdog, etc.).

    It also sounds like when you are not using CCS and letting the boot-loader run, the application does not run. What exactly is happening? Does the boot-loader run at all? Does it run and not find the application image? Does it not jump properly to the application image?

    Todd

  • Additionally,

    - What TI software (and version) are you using? 

    - Does the boot-loader use SYS/BIOS?

    Todd

    [8/26 update: Marking this as TI Thinks Resolved due to no response from original poster.]