This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Could the CCS be extended to support other MCU online ?

Other Parts Discussed in Thread: CC2640

Tool/software: Code Composer Studio

Hi, every one:

There is a CCS installed instance that support CC2640 development in my computer. I hope extend it to support other. I don't want to re-install a CCS instance, and want to extend it to support CC32xx with online installation. How should I do ?

  • Robin,

    If you run the same CCS installer again and point it to your existing installation it will allow you to add support for additional device families.  It is not going to do a full re-install, it will just run the component installers for the items that need to be updated.

    Regards,

    John

  • Thanks, John:

    I use CCS menu command 'Help -> Install New Software', in the new software dialog, I set the 'Work with:' to '--All Available Sites--', then I can see some devices support such as 'CC2640'. But I can not find online installation for 'CC32xx Device Support'.

    Anyway, I will follow your suggest.

    Best regard

    Robin

  • Robin,

    In general the "install new software" feature won't support adding new device families.  This is because often installing support for a new family requires other components that are not part of the device support package.

    Regards,

    John