Other Parts Discussed in Thread: TMS320F280049C
Tool/software: Code Composer Studio
Hi TI Community,
I am using the TMS320F280049C device with its default RAM_lnk.cmd file and i am getting the "program will not fit into available memory" error . when i try to debug my code of pwm and Adc
the ERROR is as follow:
"../280049C_RAM_lnk.cmd", line 37: error #10099-D: program will not fit into available memory. placement with alignment/blocking fails for section ".text" size 0x11be page 0. Available memory ranges:
RAMM0 size: 0x30b unused: 0x0 max hole: 0x0
RAMLS0 size: 0x800 unused: 0xf4 max hole: 0xf4
RAMLS1 size: 0x800 unused: 0x800 max hole: 0x800
RAMLS2 size: 0x800 unused: 0x800 max hole: 0x800
RAMLS3 size: 0x800 unused: 0x800 max hole: 0x800
RAMLS4 size: 0x800 unused: 0x800 max hole: 0x800
error #10010: errors encountered during linking; "epwm_ex1_trip_zone.out" not built
>> Compilation failure
makefile:146: recipe for target 'epwm_ex1_trip_zone.out' failed
gmake[1]: *** [epwm_ex1_trip_zone.out] Error 1
gmake: *** [all] Error 2
makefile:142: recipe for target 'all' failed
**** Build Finished ****
and my CMD file
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002
RAMM0 : origin = 0x0000F5, length = 0x00030B
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x0000F3 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMLS6 : origin = 0x00B000, length = 0x000800
RAMLS7 : origin = 0x00B800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x002000
RAMGS1 : origin = 0x00E000, length = 0x002000
RAMGS2 : origin = 0x010000, length = 0x002000
RAMGS3 : origin = 0x012000, length = 0x002000
}
SECTIONS
{
codestart : > BEGIN, PAGE = 0
.TI.ramfunc : > RAMM0 PAGE = 0
.text : >>RAMM0 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4, PAGE = 0
.cinit : > RAMM0, PAGE = 0
.pinit : > RAMM0, PAGE = 0
.switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM1, PAGE = 1
.ebss : > RAMLS5, PAGE = 1
.econst : > RAMLS5, PAGE = 1
.esysmem : > RAMLS5, PAGE = 1
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS1, PAGE = 1
}
can you please explain me who is the Problem
best regards
YT