Tool/software: Code Composer Studio
Hello,
I use the code composer studio Version: 9.1.0.00010. I have not installed the SDK and the other TI specific software components in the folder c:\ti. I made the needed CCS settings and imported the additonal parts like the SDK. I did that on two computers.
On one computer I installed the TI specific components in e:\ti. When I open TiRex i can browse through the examples but I can't copy the examples into my workspace. The CCS shows me the folling dialogue again and again.
The following picture shows my settings Window -> Preferences -> Code Composer Studio -> Product. If I press the button Rediscover the CCS imports the installed components.
If I remeber correctly I also had to do this on the othert PC as well, if I changed the workspace folder.
My question: Is there a possibility to make these settings "really" persistent?