Other Parts Discussed in Thread: MSP430WARE
Tool/software: TI C/C++ Compiler
Hello,
I'm trying to restore a very old project - MSP430F5259, TI-RTOS based, built circa 2015/6.
I've installed the latest TI-RTOS(2.20) / MSPWare (3.80.03.07) /CCS (v901) / xdctools (3.55.02.22) and pulled the source and project files from git.
I just can't get it to build properly.
I'm afraid that I'm experiencing a mess-up between older and current versions of the dev tools/libraries etc and probably system 'macros' (aka 'variables' such as ${COM_TI_MCU_MSP430WARE_LIBRARY_PATH}) are probably irrelevant...
Is there a way / clear guide of how to prepare a clean build environment comprising the ide (ccs), rtos, xdctools and supporting MSPware libraries (or are these part of the RTOS distribution) + sys 'variables', and what are their interdependencies - e.g. which versions work with which, is there a forward compatibility, driverlib & iqmathlib location (MSPware folders or TI RTOS folders) etc etc..
What is the correct way to recover an old project as I'm spending hours and hours to no avail :-(
Thanks