I have updated CCS with the updater. I can't remember which updates I got but now I have problems when I try to debug. The project is the same I used before and with the same Target configuration file (Black Hawk USB2000 and F28035). The error is that I'm missin flashing tool. And if I go to debug window, it shows that I have TMS192C2006 Gel file loaded and it doesn't help if I load the f28035.gel file. Which setting is now wrong?
Edit: Some times it helps to restart the CCS4 and then it works for that session.