This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LC4357: Error #128 expected a statement

Part Number: TMS570LC4357

Tool/software: Code Composer Studio

Hi there,

I am learning coding ARM with CCS, trying to follow the training "How to Tutorial: turning on the LEDs" https://training.ti.com/hercules-how-tutorial-turning-leds?cu=1136292.

Codes in the HL_sys_main.c is attached,

/** @file HL_sys_main.c 
*   @brief Application main file
*   @date 11-Dec-2018
*   @version 04.07.01
*
*   This file contains an empty main function,
*   which can be used for the application.
*/

/* 
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com  
* 
* 
*  Redistribution and use in source and binary forms, with or without 
*  modification, are permitted provided that the following conditions 
*  are met:
*
*    Redistributions of source code must retain the above copyright 
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the 
*    documentation and/or other materials provided with the   
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/


/* USER CODE BEGIN (0) */
#include "HL_het.h"

/* USER CODE END */

/* Include Files */

#include "HL_sys_common.h"
#include "HL_system.h"


/* USER CODE BEGIN (1) */
/* USER CODE END */

/** @fn void main(void)
*   @brief Application main function
*   @note This function is empty by default.
*
*   This function is called after startup.
*   The user can use this function to implement the application.
*/

/* USER CODE BEGIN (2) */
/* USER CODE END */

int main(void)
{
/* USER CODE BEGIN (3) */
    /*set HET port pins to output*/
    gioSetDirection(hetPORT1, 0xFFFFFFFF);

        /*set white NHET LEDs high */
        /*there are 2 more LED's */
    gioSetBit(hetPORT1, 0, 1);
    gioSetBit(hetPORT1, 5, 1);
    gioSetBit(hetPORT1, 17, 1);
    gioSetBit(hetPORT1, 18, 1);
    gioSetBit(hetPORT1, 25, 1);
    gioSetBit(hetPORT1, 27, 1);
    gioSetBit(hetPORT1, 29, 1);
    gioSetBit(hetPORT1, 31, 1);

    /*infinite loop */
    while(1)
/* USER CODE END */
}

/* USER CODE BEGIN (4) */
/* GIO interrupt notification (Not used but must be provided) */
void gioNotification(int bit)
{
    return;
}
void esmGroup1Notification(int bit)
{
    return;
}
void esmGroup2Notification(int bit)
{
    return;
}


/* USER CODE END */
then I encountered some errors that I can not solve.

Could someone give me some basic lessons on this goal ?

thanks a lot.

  • Hello,

    The semi-colon at the end of the while(1) statement on line 88 is missing.

    Thanks

    ki

  • Hi Ki

    Sorry didn't see that small typo.

    now the GIO_LED.out file is being built. it still gets frozen at the automatic library build, see pic.

    does this have something to do with the while(1) loop ?

  • Lu Zheng said:
    now the GIO_LED.out file is being built. it still gets frozen at the automatic library build, see pic.

    It is building the required run-time library. This is a one time thing for each compiler installation. This can take a long time, even for high performance machines. Please be patient and let it build.

    Lu Zheng said:
    does this have something to do with the while(1) loop ?

    No

    Thanks

    ki