Other Parts Discussed in Thread: MSP430F2274
Hi, I'm running CC 4.2 under Windows 7, targeting the MSP430F2274. My issue is that I cannot seem to get pointers to work other than chars. I've tried various standard ANSI C examples. When I try to set a pointer to a value, nothing appears in memory from what I see in the memory monitor. When I try to print the value pointer, it prints different random garbage. I can successfully print the address of the pointer. And I can manually set its value in memory using the monitor. But I can't set a value in C nor can I read, manipulate or print a value. Tests using conditional statements confirm what the memory monitor is telling me that only char pointers work. Any help appreciated,
Thanks,
- Chris