Hi, this is a minor issue I'm having with CC 4.2 under Win7. But it concerns me enough that I'd like an explanation. While working in debug mode, CC frequently creates multiple instances of my .c source files (ie, of the same .c file) in separate tabs in the debug source code pane. One instance may reflect code changes and/or breakpoints and the other won't. How can I prevent this from happening? Is it OK to delete these redundant panes as they're created? Which version should I edit or set breakpoints in? Thanks.