I have an issue that I assumed was minor but I'll bring it up. Perhaps it explains some of the flaky behavior I've seen (see previous posts). When I compile I get a warning saying that the project was created with CC 3.3.1 and recommending that I migrate the project to the current version (if I'm interpreting it right). Problem is I've so far been unable to migrate or import this project or my other projects into CC 4.2 Using the Import function, I can point it right to the project folder inside the workspace folder and it simply doesn't see it. It's looking for a .pjt file but there are no such files. I've tried importing it as a 3.x project as well as a 4.x project. I assumed that because I'm running 4.2 that all of the 4.2 tools (comp+link) are being used. Now I'm really not so sure what's going on...ideas?