Hello Forum,
this is a repost from an other forum into which i posted by error.
Recently I came across a strange behaviour to that I want a comment please.
Environment: CCS4 under WinXP for C2000
I have a main.c with some global variables defined there like:
Uint16 Variable1;
enum { ..., A, B, ... } Variable2;
Both variables are reused in a file subroutines.c.
I did there the follwing mistake:
extern Uint32 Variable1; (- instead of Uint16)
extern enum { ..., B, A, ...} Variable2; (- instead of A,B)
CCS4 silently compiled several times ignoring the mismatches until I found the difference using the debugger.
I retested that again and the compiler still does not show any errors or warnings.
Is this intentionally or are there any compilerflags to find such inconsistencies?
rgds
FJ