This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100v2 can't connect to omapl138evm on linux ubuntu 10.04



Hello I've just installed CCS v5 (5.0.0.00095) on Linux Ubuntu x86_64 10.04.

Trying to connect to my omapl138evm I got :

 

Texas instrument XDS100v2 USB Emulator_0/xxxxxxx_0 (Disconnected: Unknown)

 

And i can't debug my target. Seems CCS can't conenct to my target via jtag.

Udev rule are installed, everything seeems fine, but I can find where node is created in /dev?

Any idea?

dev@dev-laptop:/dev/bus/usb$ cat /etc/udev/rules.d/71-sd-permissions.rules
# Spectrum Digital USB devices
SUBSYSTEM=="usb", ATTR{idVendor}=="0c55" ,ATTR{idProduct}=="0540", ATTR{manufacturer}=="Spectrum Digital Inc.",MODE="0666"
SUBSYSTEM=="usb", ATTR{idVendor}=="0c55" ,ATTR{idProduct}=="0510", ATTR{manufacturer}=="Spectrum Digital, Inc.",MODE="0666"
SUBSYSTEM=="usb", ATTR{idVendor}=="0c55" ,ATTR{idProduct}=="2000", ATTR{manufacturer}=="Spectrum Digital, Inc.",MODE="0666"
SUBSYSTEM=="usb", ATTR{idVendor}=="0c55" ,ATTR{idProduct}=="0562",MODE="0666"

dev@dev-laptop:/dev/bus/usb$ cat /etc/udev/rules.d/71-ti-permissions.rules
SUBSYSTEM=="usb",ENV{DEVTYPE}=="usb_device",ATTRS{idVendor}=="0403",ATTRS{idProduct}=="a6d0",MODE:="0666"

dev@dev-laptop:/dev/bus/usb$ lsusb
Bus 005 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 004 Device 002: ID 0b05:1712 ASUSTek Computer, Inc. BT-183 Bluetooth 2.0+EDR adapter
Bus 004 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 003 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 002 Device 002: ID 0403:6001 Future Technology Devices International, Ltd FT232 USB-Serial (UART) IC
Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 001 Device 009: ID 0403:a6d0 Future Technology Devices International, Ltd
Bus 001 Device 004: ID 2001:3c05 D-Link Corp. [hex] DUB-E100 Fast Ethernet [asix]
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

and finally:

dev@dev-laptop:/dev/bus/usb$ udevadm info -a -p  $(udevadm info -q path -n /dev/bus/usb/001/009)

Udevadm info starts with the device specified by the devpath and then
walks up the chain of parent devices. It prints for every device
found, all possible attributes in the udev rules key format.
A rule to match, can be composed by the attributes of the device
and the attributes from one single parent device.

  looking at device '/devices/pci0000:00/0000:00:1d.7/usb1/1-1':
    KERNEL=="1-1"
    SUBSYSTEM=="usb"
    DRIVER=="usb"
    ATTR{configuration}==""
    ATTR{bNumInterfaces}==" 2"
    ATTR{bConfigurationValue}=="1"
    ATTR{bmAttributes}=="80"
    ATTR{bMaxPower}=="400mA"
    ATTR{urbnum}=="12"
    ATTR{idVendor}=="0403"
    ATTR{idProduct}=="a6d0"
    ATTR{bcdDevice}=="0700"
    ATTR{bDeviceClass}=="00"
    ATTR{bDeviceSubClass}=="00"
    ATTR{bDeviceProtocol}=="00"
    ATTR{bNumConfigurations}=="1"
    ATTR{bMaxPacketSize0}=="64"
    ATTR{speed}=="480"
    ATTR{busnum}=="1"
    ATTR{devnum}=="9"
    ATTR{version}==" 2.00"
    ATTR{maxchild}=="0"
    ATTR{quirks}=="0x0"
    ATTR{authorized}=="1"
    ATTR{manufacturer}=="SD"
    ATTR{product}=="Texas Instruments Inc.XDS100 Ver 2.0"
    ATTR{serial}=="SDSMA1NM"

  looking at parent device '/devices/pci0000:00/0000:00:1d.7/usb1':
    KERNELS=="usb1"
    SUBSYSTEMS=="usb"
    DRIVERS=="usb"
    ATTRS{configuration}==""
    ATTRS{bNumInterfaces}==" 1"
    ATTRS{bConfigurationValue}=="1"
    ATTRS{bmAttributes}=="e0"
    ATTRS{bMaxPower}=="  0mA"
    ATTRS{urbnum}=="155"
    ATTRS{idVendor}=="1d6b"
    ATTRS{idProduct}=="0002"
    ATTRS{bcdDevice}=="0206"
    ATTRS{bDeviceClass}=="09"
    ATTRS{bDeviceSubClass}=="00"
    ATTRS{bDeviceProtocol}=="00"
    ATTRS{bNumConfigurations}=="1"
    ATTRS{bMaxPacketSize0}=="64"
    ATTRS{speed}=="480"
    ATTRS{busnum}=="1"
    ATTRS{devnum}=="1"
    ATTRS{version}==" 2.00"
    ATTRS{maxchild}=="8"
    ATTRS{quirks}=="0x0"
    ATTRS{authorized}=="1"
    ATTRS{manufacturer}=="Linux 2.6.32-25-generic ehci_hcd"
    ATTRS{product}=="EHCI Host Controller"
    ATTRS{serial}=="0000:00:1d.7"
    ATTRS{authorized_default}=="1"

  looking at parent device '/devices/pci0000:00/0000:00:1d.7':
    KERNELS=="0000:00:1d.7"
    SUBSYSTEMS=="pci"
    DRIVERS=="ehci_hcd"
    ATTRS{vendor}=="0x8086"
    ATTRS{device}=="0x27cc"
    ATTRS{subsystem_vendor}=="0x1043"
    ATTRS{subsystem_device}=="0x1237"
    ATTRS{class}=="0x0c0320"
    ATTRS{irq}=="23"
    ATTRS{local_cpus}=="00000000,00000003"
    ATTRS{local_cpulist}=="0-1"
    ATTRS{modalias}=="pci:v00008086d000027CCsv00001043sd00001237bc0Csc03i20"
    ATTRS{numa_node}=="-1"
    ATTRS{broken_parity_status}=="0"
    ATTRS{msi_bus}==""
    ATTRS{companion}==""

  looking at parent device '/devices/pci0000:00':
    KERNELS=="pci0000:00"
    SUBSYSTEMS==""
    DRIVERS==""

Can anyone help?