Part Number: CCSTUDIO
Tool/software: Code Composer Studio
Hi,
I am having troubles with running unit tests on target using Parasoft C++test plugin. It is using scripting to connect to the debug server and I managed to bypass the use of ccs variables replacing them with actual paths, but the original problem persists. These specific variables seem to be missing at my version of CCS (Code Composer Studio 9.0.1):
${ccs:connector_cmd_line}
${ccs:active_target_config}
The other ones like ${cpptest:cfg_dir} are resolved to the actual paths, but the ones above stay not resolved.
Maybe Parasoft uses ccs variables no longer used in newer ccs versions. But I would like to understand the syntax of using these variables. I have found no information on the Internet on any list of ccs variables available for use. The only place was CCS build settings and showing system variables, but these are simple variables with no colon in the middle of the variable.
Where can I find any documentation on this and what is the meaning of the colon between "ccs" and the second part of variable name? Is this some sort of a namespace?
Cheers.