This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi everyone,
I need to use tms320c6678-evm as an external host to configure AWR1243 . According to the instructions in the html , I am trying to write interface functions . I have encountered the following warning :
Description Resource Path Location Type
#515-D a value of type "ti_sysbios_knl_Semaphore_Handle *" cannot be assigned to an entity of type "osiLockObj_t *" host_driver.c /AWR1243_V5/1243/user_define line 153 C/C++ Problem
The warning code is as follows:
osiLockObj_t* pLockObj;
Semaphore_Handle timerSemaphore;
pLockObj = &timerSemaphore ;
In order to resolve this warning, I tried to repeat it in visual studio. So I wrote the following code:
#include <stdio.h>
#include <string.h>
struct ti_sysbios_knl_Semaphore_Object {
int i;
char dummy;
};
typedef struct ti_sysbios_knl_Semaphore_Object ti_sysbios_knl_Semaphore_Object;
typedef ti_sysbios_knl_Semaphore_Object* ti_sysbios_knl_Semaphore_Handle;
#define Semaphore_Handle ti_sysbios_knl_Semaphore_Handle
typedef void* HANDLE;
typedef HANDLE osiLockObj_t;
int main(void) {
Semaphore_Handle timerSemaphore;
osiLockObj_t * pLockObj;
pLockObj = &timerSemaphore;
return 0;
}
The same program can be compiled in VS, but not compiled in CCS. Where is the problem?
Best wishes!
Tf