This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443BOOST: CCS9.1 Load program issue

Part Number: IWR1443BOOST


Tool/software: Code Composer Studio

Hi

I started getting below error since last couple of days and unable to figure out reason behind it.

I usually load config and connect target and load program. I tried on multiple eval kits and also different .xer4f files.

I also uninstalled CCS couple of items and did fresh installation but couldn’t get rid of below error.

Any suggestion to resolve this error ?  Quick response to this is highly appreciated.

 Cortex_R4_0: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x3c: (Error -1065 @ 0x0) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.2.0.00004)

Cortex_R4_0: File Loader: Verification failed: Target failed to write 0x00000000

Cortex_R4_0: GEL: File: C:\Users\Software\TI\xwr14xx_mmw_mss.xer4f: Load failed.

  • Hi,

    When these issues happen, I tend to look for the common denominator across all the scenarios. As I understood from your question, it seems the same code/project is failing on multiple boards and even across CCS installs. 

    In this case, my suspicion falls in the project itself. Especially given the error message talks an issue when trying to write to address 0x0 (which in this device is ROM code). 

    Additional details can be found at section 9.7.2 of the CCS User's Guide - if you have CCSv9.1, you can access it via the Help (menu Help --> Contents). 

    Otherwise, check:

    http://software-dl.ti.com/ccs/esd/documents/users_guide/index.html 

    Hope this helps,

    Rafael