I have a a customer with the following problem - I've seen a few posts with similar problems but not exactly the same. They are using a 6747 and CCS V4.
I compile and build the executable .out file in the DOS command window. Then I create a “Standard Make Project” in the CCS, and a target configuration file. To test the code, I select “Debug Active Project” under “Target” menu. CCS is supposed to load the .out file to the target, and halt the CPU. But After I select “Debug Active Project”, it does not halt the CPU, and the “Terminate All” button is on.
Any help would be appreciated.
Cheers
Calum