Part Number: TMDSEMU200-U
Other Parts Discussed in Thread: TM4C1290NCPDT
Tool/software: Code Composer Studio
Hi,
I'm using the XDS200 debugger with TM4C1290NCPDT. I have started statistical profiling at 1024 sampling,
120 MHz clock. Not sure what is the best sampling to use?
I am debugging an external reset issue (which will trigger at 1.6 seconds of inactivity in the watchdog toggle
pulse). What is the length of this SWO trace buffer? Will it save instructions for the past 3 seconds or something like that?
If this buffer is much shorter, I have external hardware to trigger an ISR as well.
Thanks,
Priya