Part Number: TMDSEMUPROTRACE
Tool/software: Code Composer Studio
Hello,
We are using for the 1st time a XDS560v2 PRO TRACE on a 60 pin connector to debug a C6657 and I have some questions about it
1-Is there a way to test the link with the DSP from the signal integrity point of view ? (I know that lauterbach probes can do an eye diagram on ARM ETM links)
2-For a PC TRACE, why CCS let us decide the number of emu pins to use ? What is the consequence of using more or less pins ?
3-Is it possible to save a PC TRACE on hard disk for future analysis ? What is the space needed per minute of recording ?
Regards,
David