This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi
I'm planning to use the TM4C1294NCPDT MCU on my costume made PCB where I need to add to my PCB some pins for debugging,
So i thought if i can use the EK-TM4C1294XL Stellaris debugger through the on board X1 terminals for programming of an external MCU.
I tried to test this between two different EK-TM4C1294XL boards but i get error communication as in the pictures below, so is there any suggestions?
Hi,
Page 4 of the EK-TM4C129XL Rev D Schematics mention that you need to remove the 0Ω resistors to debug a MCU outside of the board. This is expected as the built-in TM4C129 device will impact the JTAG communications.
Hope this helps,
Rafael
So I understood that there is no issues with the used connections, right?
because if the problem is in the 0 OHM only so the there will be no problem to use these X1 terminals in my costume made PCB.
BR
Hani
Hani,
The connections themselves are not a problem. Just keep in mind they need to be as short as possible to avoid any communcations issues.
Regards,
Rafael