Part Number: AWR1843BOOST
Tool/software: Code Composer Studio
Hi,
I am trying to test odoc_CAN demo from 2.1.0.04 of SDK. It always fails with something like maybe mailbox exeption. I tried adding some debug logs this is my debug output . How do i solve this exception. I am using CAN_Classic and added this printf statement to Can_Transmit_Schedule() fn to check simultaneously whether CAN is fine or not.
[Cortex_R4_0] **********************************************
Debug: Launching the Millimeter Wave Demo
**********************************************
Debug: MMWDemoMSS Launched the Initialization Task
Debug: MMWDemoMSS mmWave Control Initialization was successful
Debug: CLI is operational
Sensor has been stopped
Debug: MMWDemoMSS Received CLI sensorStart Event
Testng
Msg:ŸåðŸåðŸåðŸåðŸåðŸåðŸå°ñå¬#Msg_id:c1 len:40
Msg:ðŸåðŸåðŸåðŸåðŸåðŸåðŸå°ñå¬#Msg_id:d1 len:8
Msg:Msg_id:d1 len:1072
Msg:ŸåðŸåðŸåðŸåðŸåðŸåðŸå°ñå¬#Msg_id:d2 len:8
Msg:Msg_id:d2 len:512
Msg:åðŸåðŸåðŸåðŸåðŸåðŸå°ñå¬#Msg_id:d3 len:8
Msg:Msg_id:d3 len:512
Msg:ŸåðŸåðŸåðŸåðŸåðŸå°ñå¬#Msg_id:d6 len:8
Msg:Msg_id:d6 len:24
Msg:åðŸåðŸåðŸå°ñå¬#Msg_id:b1 len:16
xdc.runtime.Main: "platform/mmwave_xwr16xx.c", line 1342: assertion failure
xdc.runtime.Error.raise: terminating execution