G'day Guys,
i seem to have a problem which i cant seem to fix.
I just purchased a TMDSDOCKF28335 deflino microcontroller and am having trouble with code composer v3.3. What happens is when i install the code composer it installs fine with or without DSP/BIOS and then when i run the CCS set-up and choose my chip that seems to work fine and then after i save and quit, CCS will open. But then if i try to run CCS by itself, the program does not want to start. It tries to run the set-up again and if you click yes or no it comes up with the error:
"Error reading Code Composer Set-up Information. Code composer may not have been correctly installed".
Just wondering if anyone can help me with this problem,
Cheers