Part Number: CC1352R
Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
Hi,
I have
CCS9.1.0
simplelink_cc13x2_26x2_sdk_320_00_68 SDK, compiler 18.12.3, XDCtools 3.55.2.22 (I've tried all the versions from 3.50 up), SYS/BIOS 6.76.2.02
"Description Resource Path Location Type
can't locate file 'C:/ti/simplelink_cc13x2_26x2_sdk_3_20_00_68/kernel/tirtos/packages/ti/sysbios/rom/cortexm/cc13xx/golden/undefined/undefined_link_ti.xdt' along the path: C:\ti\simplelink_cc13x2_26x2_sdk_3_20_00_68\kernel\tirtos\packages\ti\platforms\simplelink;C:/ti/simplelink_cc13x2_26x2_sdk_3_20_00_68/source;C:/ti/simplelink_cc13x2_26x2_sdk_3_20_00_68/kernel/tirtos/packages;C:/ti/simplelink_cc13x2_sdk_2_30_00_45/source;C:/ti/simplelink_cc13x2_sdk_2_30_00_45/kernel/tirtos/packages;C:/ti/ccs910/xdctools_3_55_02_22_core/packages;..; .xdchelp /Basic line 94 C/C++ Problem"
What's with the "../undefined/undefined/undefined_link_ti.xdt"
I've yet to get a successful build for numerous reasons which required intervention, but this one isn't something I can fix.
Thank you!
John