Part Number: IWR6843ISK
Tool/software: Code Composer Studio
Hi,
I am using import field in project-spec to import another project-spec. Also I am using references to create build dependencies. Both the project have same two build configurations(Debug Release). CCS is able to Import both the projectspecs successfully and create the build dependencies. How-ever the dependency configuration selected for the dependent project is "Active" and not respective Debug and Release. There is no issue with the project-spec since if the dependent project is already imported in work-space and then if I import the parent project-spec the build dependencies are properly created. I tested it with CCS 8.3 and CCS 9.1. Is this known issue or expected behavior.
Thanks
Yogesh