This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/EK-TM4C1294XL: CCS 9.2.0.00013 Linker command file list in project properties doesn't order devices

Part Number: EK-TM4C1294XL


Tool/software: Code Composer Studio

With CCS 9.2 if create a new project where fail to select a linker command file, then can set the linker command file used in the project properties after the project has been created.

A minor issue is that the list of available linker command files displayed from the project properties isn't ordered which makes finding the required device fiddly:

Can the list of linker command files be ordered to help finding the required one?

  • Chester,

    Thanks for reporting this. In all fairness, CCSv9.1.0, 8.3.0 and 8.2.0 also show this behaviour for me - perhaps you could call it a 'feature'? :)

    At any rate, I filed the bug report CCSIDE-3702. Please check its status in the link SDOWP in my signature below. 

    I apologize for the inconvenience, 

    Rafael