Tool/software: Code Composer Studio
I upgraded CCS 9.1 under Debian linux 10.1 to 9.2 The upgrade changed the splash screen but the following now seem to try connecting to local host.
"CCS App Center"
"Resource Explorer"
I know this because after it first happened I fired up the application wireshark and I retried both of the applications, with them going to local host with the "Resource Explorer" continuously and "CCS App Center" for a few tried attempts then complaining it can't connect. It does not appear to be trying to connect to a TI website.
So is this a configuration issue? If yes where do I fix the location these two applications are trying to connect?
Thanks ahead of time.
Attached is the image of the CCS App Center.
I also attached the wireshark log.https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/81/2019_5F00_1014_5F00_01_5F00_localhost.pcapng.7z