This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"Connect to PRSC failed" error with CCSv4.2

Greetings,

I am getting following error while connecting to a C64x+ DSP:

Error connecting to the target:
Connect to PRSC failed

 

I am getting this error wile connecting C6457, C6474, C6472 and C64x+ dsp of DM6446.

 

If I retry after restarting CCS and my board several times, I am able to connect to the board, but I do not understand the reason behind this error.

And this error pop-ups intermittently without any reason.

 

Please note that I am able to connect to the ARM9 CPU with DM6446 but get the above error while connecting the 64x+ DSP.

This error did not turn up on CCSv4.1 and earlier.

Am I missing any thing?

 

Thanks,

Amitkumar Solanki