Other Parts Discussed in Thread: TMS320F28335, CCSTUDIO
Hi All,
I am new to Tms320f28335 and I am working on eZdsp Kit of Tms320f28335 and using CCStudio 3.3 software for building up the code. I had written a simple program to toggle the LED. I had programmed it by using USB JTAG provided with the kit. It is working properly, but the program is executed from the SARAM region in the controller. Later on I found the utility called as SD Flash to program the Flash. But I am not getting it. I tried to make changes in the command file, it compiles it successfully but when I try it to program through USB JTAG it gives an error that "Data verification failed at address 0x300000". Is there anything that I am missing or doing wrong ? Or the CCStudio or the eZdsp Kit doesnt allow to program the Flash ?
Thanks in Advance,
Iqbal SIngh