This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430G2553: CCS/MSP430G2553

Part Number: MSP430G2553


Tool/software: Code Composer Studio

I have a micro-controller which is msp430G2553 with a captouch.

If I press the center button on the captouch, the LED should be on.

Here is the introduction:

Use 2 threshold values, and keep track of the latest button status. If the button is currently not being pressed, you are comparing the latest samples with a "lower" threshold value. If it is lower than it, change the button status to "pressed". If the latest button status is "pressed", then you compare latest samples with a "higher" threshold value. If it is higher than it, then change the button status to "not pressed". This effectively gives you a "noise margin". Any samples that are between the 2 threshold values are basically ignored - these would be samples that come in when you are halfway through pressing the button.

The LED should TOGGLE each time the button is pressed. You will need a SW debouncing mechanism.

I got my base_line address which is 0xD3. Also, when I am not touching the pad, it gives me 0xD0. When I am touching the pad, it gives me C0.

I know I need to subtract 4 and 10 from the base line to set two threshold values. 

But, I am struggling with expressing the assembly code.

Could you help me out?

;-------------------------------------------------------------------------------
; MSP430 Assembler Code Template for use with TI Code Composer Studio
; Toggles the center LED when center "key" on the capacitive touch sensor
; is "pressed"
;-------------------------------------------------------------------------------
.cdecls C,LIST,"msp430.h" ; Include device header file
SWdelay .equ 0x0006 ; delay value used by the SW timer
;-------------------------------------------------------------------------------
; Allocate 2 bytes for the baseline measurement
;-------------------------------------------------------------------------------
.data
.bss meas_base, 2 ;
;-------------------------------------------------------------------------------
; Allocate another 2 bytes for the latest measurement
;-------------------------------------------------------------------------------
.bss meas_latest, 2 ;
;-------------------------------------------------------------------------------
.text ; Assemble into program memory
.retain ; Override ELF conditional linking
; and retain current section
.retainrefs ; Additionally retain any sections
; that have references to current
; section
;-------------------------------------------------------------------------------
RESET mov.w #__STACK_END,SP ; Initialize stackpointer
StopWDT mov.w #WDTPW|WDTHOLD,&WDTCTL ; Stop watchdog timer
;-------------------------------------------------------------------------------
; Main loop from here
;-------------------------------------------------------------------------------
; Setting up P1.0 to drive center LED
;-------------------------------------------------------------------------------
bis.b #0xff, &P1DIR ; set up P1 as outputs
bic.b #0xff, &P1OUT ; P1 outputs 0
;-------------------------------------------------------------------------------
; Setting up P2.5 to pin oscillation mode
;-------------------------------------------------------------------------------
bic.b #BIT5,&P2DIR ; P2.5 input
bic.b #BIT5,&P2SEL ;
bis.b #BIT5,&P2SEL2 ;
;-------------------------------------------------------------------------------
; The oscillation from P2.5 is driving INCLK input of TA0
; No division of this clock source
;-------------------------------------------------------------------------------
mov #TASSEL_3, &TA0CTL ;
;-------------------------------------------------------------------------------
; Setting up to capture the value of TAR on either rising or falling edges
; using SW based trigger
;-------------------------------------------------------------------------------
mov #CM_3 + CCIS_2 + CAP, &TA0CCTL1 ;
;-------------------------------------------------------------------------------
; Get the baseline reading
;-------------------------------------------------------------------------------
; Clear TAR and start TA0 in continuous mode; use BIS and not MOV
; so that you don't cancel previous settings
;-------------------------------------------------------------------------------
bis #MC_2 + TACLR, &TA0CTL ;
;-------------------------------------------------------------------------------
; Call the SW delay routine, which here it is used to provide the accumulation
; period; could use instead ACLK fed from VLO
;-------------------------------------------------------------------------------
call #SWtimer ;
;-------------------------------------------------------------------------------
; Now, after the accumulation period has passed, generate a SW based
; capture trigger by toggeling CCIS0
;-------------------------------------------------------------------------------
xor #CCIS0, &TA0CCTL1 ;
;-------------------------------------------------------------------------------
; Save the baseline captured value in meas_base
;-------------------------------------------------------------------------------
mov TA0CCR1, meas_base ; note the use of the SYMBOLIC AM
bic #MC1+MC0, &TA0CTL ; Stop TA
sub #2, meas_base ; Adjust the baseline
;-------------------------------------------------------------------------------
; From here on check again and again the status of the sensor
; If it was "pressed", i.e. meas_latest =/= meas_base, toggle the central LED
;-------------------------------------------------------------------------------
CheckAgain bis #TACLR, &TA0CTL ; Clear TAR
bis #MC_2, &TA0CTL ; Continuous Mode
call #SWtimer ;
xor #CCIS0, &TA0CCTL1 ;
mov TA0CCR1, meas_latest ;
bic #MC1+MC0, &TA0CTL ;
cmp meas_latest, meas_base ;
jeq NoKey ;
xor #1, P1OUT ; Toggle center LED if key "pressed"
NoKey nop ; Could do a lot of useful things here
; Do something here for key "not pressed"
jmp CheckAgain ;
;-------------------------------------------------------------------------------
SWtimer: mov #SWdelay, r6 ; Load delay value in r5
Reloadr5 mov #SWdelay, r5 ; Load delay value in r6
ISr50 dec r5 ; Keep this PW for some time
jnz ISr50 ; The total SW delay count is
dec r6 ; = SWdelay * SWdelay
jnz Reloadr5 ;
ret ; Return from this subroutine
;-------------------------------------------------------------------------------
; Stack Pointer definition
;-------------------------------------------------------------------------------
.global __STACK_END
.sect .stack

;-------------------------------------------------------------------------------
; Interrupt Vectors
;-------------------------------------------------------------------------------
.sect ".reset" ; MSP430 RESET Vector
.short RESET