Hi,
I used to run some Debug Server Scripting on OMAP4430 TEB .
The script is based on the load_ti javascript.
It connects to the cortex a9_0 and loads one application. this application loads the cortex M3_0 program.and launch its execution
With the CCSV4.2 CR1 release, it sounds the ducati code is not loaded correctly.
Same script / executable is working fine on CCSV4.2 M9
rgds