This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC1352P: SDK 3.30.00.03 Exampls complain about XDCtools 3.60.999 even with CCS 9.01.0004. (SDK3.20.00.68 worked fine)

Part Number: LAUNCHXL-CC1352P

Tool/software: Code Composer Studio

When I try to import example projects from SimpleLink CC13x2 26x2 SDK - V 3.30.00.03 I receive this error:
        "No XDCtools, equivalnet to the specified version '3.60.999', are available - defaulting to '3.55.0.11_core"

I have Code Composer Studio Version 9.01.0004 but see no way to install XDCtools 3.60.999.  I'm not sure if doing so would be the solution.

The projects import but fail to compile with a message:
        "Error: Configurable "$hardware" of "/ti/drivers/PIN" is of an unknown schema type"

The examples worked perfect when my resource explorer had SDK 3.20.00.68 but it seems to have automatically upgraded .