This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler: Odd behavior with nested lambdas, SFINAE, and name lookup



Tool/software: TI C/C++ Compiler

Hi

I recently stumbled upon an odd compiler error. I was able to reduce the code to the following program that shows the same behavior:

#include <utility>

using std::declval;

template<typename F, typename T> struct Test
{
    enum { value = sizeof(declval<F>()(declval<T>()), 0) };                 // 1
    // enum { value = sizeof(std::declval<F>()(std::declval<T>()), 0) };    // 2
};

template<typename F, typename T> void call(F&& f, T t)
{
    (void) Test<F, T>::value;
    f(t); // not actually needed
}

int f()
{
    int n = 0;

    call([&n](auto) {                                                       // 3
        call( [&n](auto) {                                                  // 4
            n += 1;
        }, 0);
    }, 0);

    return n;
}

As given, the code compiles with at least gcc and clang, whereas the TI C6000 compiler (8.3.4) emits the following error:

"lam2.cc", line 23: error #20: identifier "n" is undefined
              n += 1;
              ^
          detected during:
            instantiation of function "lambda [](auto)->auto [with
                      <auto-1>=int]" at line 7
            instantiation of class "Test<F, T> [with F=lambda [](auto)->auto,
                      T=int]" at line 13
            instantiation of "void call(F &&, T) [with F=lambda [](auto)->auto,
                      T=int]" at line 13
            instantiation of "void call(F &&, T) [with F=lambda [](auto)->auto,
                      T=int]" at line 21

1 error detected in the compilation of "lam2.cc".

>> Compilation failure

I made a number of observations that only make the problem seem weirder:

  • If you comment out the line marked "1" and uncomment the line marked "2", the code compiles
  • If you replace one of the auto parameter types in either line "3" or "4" with "int", the code compiles
  • If you add a local reference "auto& nref=n;" in the lambda expression on line "3" and capture "nref" instead of "n" in line "4", the code compiles

All of that seems really odd to me, you might want to have a look at it.

Markus

  • Thank you for reporting this problem, and providing a concise test case.  I can reproduce the same result.  I filed the entry CODEGEN-6810 in the SDOWP system to have this issue investigated.  You are welcome to follow it with the SDOWP link below in my signature.

    Thanks and regards,

    -George