This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6678: PRSC module failed to write to a register

Part Number: TMS320C6678

Tool/software: Code Composer Studio

Dear,

We have used C6678 in our custom board in which we are facing the following error when system reset is issued: 

C66xx_0: Failed System Reset: (Error -6311) PRSC module failed to write to a register. (Emulation package 7.0.100.0) 

C66xx_0: Trouble Halting Target CPU
C66xx_0: Trouble Reading Register PC
C66xx_0: Trouble Reading Register ControlRegisters.CSR
C66xx_0: Trouble Reading Register ControlRegisters.CSR
C66xx_0: Trouble Reading Register ControlRegisters.CSR
C66xx_0: Trouble Reading Register ControlRegisters.CSR
C66xx_0: Trouble Reading Register ControlRegisters.CSR
C66xx_0: Trouble Reading Register ControlRegisters.CSR

We are able to connect and load the application on to DSP and execute, We are able to Boot from NOR flash on EMIF also

We have verified the DSP clocks and reset timings of DSP, All are good

Could you help us to resolve the issue..

Awaiting for you reply...!

Thanks & Regards,

Mounika Reddy