Part Number: TMS320C5505
Tool/software: Code Composer Studio
I am working on a program which required Int16 data[48000] allocation, initially the linker warns me about the .bss allocation is not successful due to memory insufficiency.
Therefore I changed the linker command file as follow:
SECTIONS
{
.text > DARAM align(32) fill = 20h { * (.text) }
/* Primary system stack */
.stack > DARAM align(32) fill = 00h
/* Secondary system stack */
.sysstack > DARAM align(32) fill = 00h
/* CSL data */
.csldata > DARAM align(32) fill = 00h
/* Initialized vars */
.data > DARAM align(32) fill = 00h
/* Global & static vars */
.bss > CE1 align(32) fill = 00h //Initially this is allocated to DARAM
/* Constant data */
.const > DARAM align(32) fill = 00h
/* Dynamic memory (malloc) */
.sysmem > DARAM
/* Switch statement tables */
.switch > DARAM
/* Auto-initialization tables */
.cinit > DARAM
/* Initialization fn tables */
.pinit > DARAM align(32) fill = 00h
/* C I/O buffers */
.cio > DARAM align(32) fill = 00h
/* Arguments to main() */
.args > DARAM align(32) fill = 00h
When the program can be compiled successfully, When I run a sample program which read data from audio in with AIC3204 and output from 3.5 audio port, I heard nothing from the output but some buzzling sound when the song is playing, when the song isn't playing, the buzzling is not there.
Can any expert explain what happen to this modification to .bss allocation?
Thank you sooo much :)))))