Part Number: TMS320C6727B
Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Hi,
I have a Spectrum Digital XDS560R I am trying to use as a JTAG emulator with CCS 3.3. I followed the instructions provided by SD (http://support.spectrumdigital.com/ccs3x_xds560r/) for both the base CCS 3.3 (no SR) and CCS 3.3 with SR 12, but did not have luck either way.
I am able to install the driver successfully according to Windows 10 64 bit, but when I try to connect over CCS, I have gotten two different errors:
(1) Failed to initialize emulator (acts as though device isn't even connected, but still lets me open CCS).
(2) Unable to load c:\ccstudio_v3.3\drivers\tixds560c6x.dvr, and will not open CCS. Note that I verified this .dvr file does exist.
I have been using the XDS510 with no issues on the same setup. However, I notice that the XDS510 setup that works is called "XDS510USB", whereas the XDS560 only provides a non-"USB" emulator option in CCSetup.
Any advice on this? I am guessing it has something to do with Code Composer being pointed to the correct files (or the correct files being given to CCS). It does look like CCS v3.3 should support this device though: http://emulators.spectrumdigital.com/files/Emulator_CCS_OS_Compatibility.pdf
Thanks,
Alec