Part Number: CC2650
Tool/software: Code Composer Studio
Hi,
I have a project for the sensortag cc2650 featuring Contiki. The project was created on CCS 6.1 where it builds perfectly well. When I try to build the project in CCS 9.2 I get a number of linker Errors in the cc26xx.ld file. See the attached screenshots below.I tried to build it in CCS9 with the same compiler version as in ccs6 (TI v5.2.2) and with a newer Version (TI v18.12.3.LTS) but I get the same errors with both compiler versions.
Any help resolving this issue would be highly appreciated!
If any more information is needed from me, let me know.
Kind regards